I have successfully created a custom bsl and an application for the msp430f5526. Both work just fine as stand alone applications. However, when I try to combine the two ti text files as a single code file, something gets lost in translation. I am able to jump to the bsl area using a cmd and it seems to intialize fine (it sends a test message over the data line as expected); however, after the first command I send to the bsl once intialized, the data line goes high and remains unresponsive.
Both ti-text files have code at location @ffd2. I am using the hex bytes for the main application at this location. Could this be whats screwing it up? Is there something special I need to do when combining ti-text files?
The project is for an SDI-12 sensor (it only has one data line) so the custom BSL and being able to jump to it from user code is absolutely necessary.
Is there a way to combine both sets of code in a single project so I can debug it like a normal person?