Hi there,
i am trying to use the I2C Bus to programm the Slave(Clock Generator).
I have pulled both SCL and SDA wires to 10kOhm and +3V3.
Problem is that the Master is not sending the correct "Slave Adress" to the slave.
I have also disconnected the wires going to the slave and measure it again and having the same results.
I did a screen shot from the SDA and SCL that was sended from the MSP432(Master):
So as far as i understood the Master starts with the START bit by pulling SDA to Low and starts the SCL Clock.
Than sends the SLAVE ADRESS so the Slave knows the message its for him. His adress its 0xD4.
So by reading the SDA i see 0xA8 and not 0xD4.
At the end of course the Slave will not pull the SDA down to Acknowledge, it stays High for None Acknowledge, or becouse the Slave knows his not the one been spoken to.
Here is also my setup code:
Any idea?