I'm loving the MSP430FR4133 Launchpad, but am new to CCS 6.1 so not sure if it's a CCS or MSP430 thing. When I run this code in debug mode it works fine, but if I power it up without being connected to CCS or press the reset button it seems stuck. It will sometimes execute some of the initial code displaying to the LCD then get stuck, or sometimes just get stuck out of the gate. How do I simply say "Debug is good, now just put the code on there without debug"?
Thanks!