I am trying to connect my MSP432 LP to a WIndows XP (32-bit) computer (having given up on using the Mac due to ongoing USB comms connection problems). I have downloaded and installed the driver package as instructed on the Energia website (XDS110_drivers.zip).
The driver installation says it was succesful however when I plug in the LP for the first time, installation of the TI debug probes driver(s) fail. The comm ports drivers install correctly.
During the driver installation these messages are shown:
"Cannot Install the Hardware
There was a problem installing this hardware:
XDS110 (02.02.04.00) with CMSIS-DAP
An error occured during the installation of the device
A service installation section in the INF is invalid"
Following this, in the Windows Device Manager, there are two devices listed as "XDS110 (02.02.04.00) with CMSIS-DAP", under "Texas Instruments Debug Probes", with yellow exclamation marks. Properties for both devices show that the driver is not installed. There are also 2 XDS110 COMM ports that are installed correctly.
I have tried this with two LP's, and two different XP computers and get the same result.
It therefore looks like there is a bug in the driver INF file somewhere.
Can anyone help? Am currently at a production standstill.
Scott