Hi Experts,
Can MSP430FR2033/2433 support 1.8V as DVCC?
In datasheet, it says that the operation range is from 1.8V to 3.3V. But it also says that the max SVS power up level is 1.99V. It seems that the SVS function cannot be disabled during LPM0 and LPM1, so the actual min operation voltage for MSP430FR2033/2433 is 2.0V. Am I right?
Thanks a lot in advance!