My R&D computer installs CCS5.1, but product line computer installs CCS5.5.
I specify my flash to a certain values in command file using "fill" keyword as follows, and generates a .out file.
MEMORY
{
......
INFODA : origin = 0x1014, length = 0x0002,fill=0x1B58 /*INV_FREQ_SET_ADDR*/
......
}
In product line CCS5.5, a dialog pops"Load program Error. a data verification error occurred." Though MCU can also run after download, 0x1014 location value is NOT 0x1B58.
In my CCS5.1, I can download the .out file to my MSP430F2417 successfully through JTAG, and 0x1014 location value is 0x1B58 as it should be.
I found a difference between these two CCS version, that is the default Erase Options. In CCS5.1, it's "Erase main and information memory", but it's "Erase main memory only".
After I modify the Erase Options in CCS5.5 to "Erase main and information memory", the download, verification and 0x1014 value are all correct.
My questions are:
1. How does the Erase Options cause this problem?
2. Is the .out file standalone? Should I copy my command file to the product line computer as well as .out file?