Other Parts Discussed in Thread: MSP-EXP430F5529LP, ENERGIA
Hi,
I am using MSP-EXP430F5529LP (eZ-FET lite) as a programmer for programming MSP430G2553 micro-controller through CCS.
I am able to debug the program but as I stop debugging and after disconnecting the launch pad when I reconnect it and power up the controller it doesn't run the code on the controller.
It seems that eZ-FET is not writing flash of MSP430G2553. Is there any way to write flash so that I can use my controller stand alone. I don't have MSP430G2553 Launch Pad, so I want to use eZ-FET lite of MSP430 F5529 launch pad.
Also is there any way to use Energia to program the MSP430G2553 micro-controller using eZ-FET lite. Can I generate some object file by compiling Energia sketch, which can be used directly to program the controller using eZ-FET lite.
Thanks