Part Number: MSP432P401R
Tool/software: Code Composer Studio
I am attempting to get the DCO to clock to it's maximum frequency of 48 MHz. However, if I use anything above 12 MHz, the debugger will begin to continually reset itself. At this point, if I try to load new code, CCS will say that the board is no longer a MSP432P401R and I have to factory reset it. Does anyone know of problems that might make this arise? Pictures and test code below. Thanks for the help.
//***************************************************************************** // // MSP432 main.c template - Empty main // //**************************************************************************** #include "msp.h" #include "driverlib.h" void main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer CS->KEY = 0x695A; CS->CTL0 |= 0x40000; CS->KEY = 0x0000; int n=0; while(1) {n++;} }