Other Parts Discussed in Thread: FDC1004, MSP430F5528, MSP430G2553
Hi there,
I am in the process of designing a system involving the fdc1004 capacitance to digital converter and would like to know what mcu people recommend.
The capacitance to digital converter will be used on a safety system to detect the proximity of a person leaning over a hand rail. (Long story short).
This hand rail is on a mobile machine and the system will be powered off a 12 volt battery source.
Required IO's from the mcu will be as follows.
- I2C to communicate with the fdc1004
- Some way to 'wake' the micro controller because it will only need to be on when an operator uses the controls on the machine.
- An output for an alarm/light. (Digital pin.)
- An output to stop the machine from operating. (Digital pin.)
The micro-controller will simply be reading the capacitance from the fdc and when the capacitance is higher than a particular value it will disable the machine from operation.
I have been using the MSP430F5528 on the launchpad development board for prototyping however I'm unsure if this is the best micro for the job.
I would appreciate any feedback on what mcu would best suit this application.
Regards,
Adam