Tool/software: Code Composer Studio
Hi,
I am getting a very strange issue on my desktop. While trying to debug any program, CCS is giving below error:
CORTEX_M4_0: Can't Run Target CPU: (Error -2134 @ 0x0) Unable to control device execution state. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
CORTEX_M4_0: JTAG Communication Error: (Error -615 @ 0x0) The target failed to see a correctly formatted SWD header. The connection to the target may be unreliable. Try lowering the TCLK setting before trying again. (Emulation package 6.0.628.3).
My version of CCS is 7.2.0.00013. I tested the issue with a sample GPIO interrupt program by TI and one of our own program. But the strange thing is, It is running fine on my colleague's system (with CCS 7.1....).
Moreover, I had one more board (same MSP432 launchpad) which I was using on my desktop, but it suddenly stopped working one day with error msg:
CCS/MSP432P401R: MSP432_Factory_Reset() cannot be evaluated. identifier not found: DP_RESET at DP_RESET=1 [msp432_factory_reset.gel:44] at MSP432_Factory_Reset()CS_DAP_0: Error connecting to the target: (Error -613 @ 0x0).
I tried to factory reset it, as per the link (e2e.ti.com/.../1854733 . But it is giving below error:
CS_DAP_0: Trouble Writing Memory Block at 0xe0044000 on Page 0 of Length 0x4: (Error -613 @ 0xE0044000) The target indicates that it is busy. Either try the SWD request again, or abort the transaction. (Emulation package 6.0.628.3)
CS_DAP_0: GEL: Error while executing MSP432_Reboot_Reset(): Target failed to write 0xE0044000@System_View at *((unsigned int *) 0xE0044000)=0x0000695A [msp432_factory_reset.gel:75] at MSP432_Reboot_Reset().
So, in short two boards are not working from the same desktop. Please help me resolve this glitch Or should I take my desktop to an Exorcist ? ; ) :D
Kind Regards
Suraj