Hi,
I would be using EVM430-I2040S for power monitoring application. It has a shunt resistance of 0.5mohm, and for a maximum current of 16A, power consumed is 0.128W (as in data sheet of EVM430-I2040S). If current in my application is close to 30A, power consumed will be less than 1W(rating of resistor used) but a large amount of heat is generated compared to the limit of 15A as specified in data sheet of evaluation kit.
So should I use another shunt resistor with a lower temperature coefficient or the one available on the evaluation kit would be fine? What is the maximum current limit for the evaluation kit?
How to connect the neutral and live wire? Should I just bring these wires and solder it to the pads available on the pcb? I have understood the configuration but I was slightly confused about the physical connections of wires.
Best Regards,
Abhishek Grover.