Tool/software: Code Composer Studio
Hello,
I have two separate projects running inside the MSP430:
- Boot
- Application
Both are loaded independently and they do not overlap in memory and handover the program flow from one to another without any problem (a lot .cmd file scripting and proxy interrupt table stuff).
My question is if it possible to do one of two things:
- Load both symbol files (Boot and Application) so I can debug with full information instead of loading just the application and whenever it jumps back to the boot I can only follow through the disassembly view.
- Merge both symbol files into one so I can load it to the debug session.
I'm using CCS.
Thank you,
Mario