Other Parts Discussed in Thread: DAC121S101EVM,
Hi, I have this launchpad kit and I am trying to mimic an energy harvesting platform. In Short, I would like to charge the supercap on the board and then have the MSP430 run off the supercap for a short time and repeat this cycle. To this end, I would like to control the voltage provided to the board. I am able to do so manually using the 3V3 Pin on the J5 header. But I am trying to find a way to do this much much faster (ideally thousands of times a second).
Could I use the DAC121S101EVM Digital to Analog convertor for this purpose? My main concern is regarding the current output of this DAC. I would have this DAC connected to a second MSP430 board and only have the VOUT from the DAC connected to my MSP DUT. From the MSP datasheet, to run at 8MHz it seems I would need 1.8mA. The DAC datasheet says it can output a max current of >50mA.
I am aware this isnt how I should be using any of this, but I'm just looking for a quick and dirty solution to mimic feeding a voltage to the MSP launchpad. If anyone has any other suggestions on how I could do this, ofcourse I would be happy to hear those as well!