Other Parts Discussed in Thread: MSP-FET, , MSP430FR6047
Tool/software: Code Composer Studio
Hi!
I am using the MSP-FET to measure the current consumption of the MSP430FR6047 via JTAG powered from the MSP-FET (3.6V). Everything works fine, except when I send data using a RF_module(3.6V) that peaks at ~70mA and is also powered from the MSP-FET. Then the time count of the EnergyTrace resets to 0 and all the graphs and battery life calculations gets messed up. I have taken a screen recording showing the issue:
The program itself does not restart or halt and the stop time of the energy trace is set to "On halt".
What could be causing the issue?
Thanks in advance!
Best regards,
Thibault