Hello,
I am just getting started with the EVM430-FR6047 eval board and am using the Ultrasonic Sensing Design Center (Water Mode). I am reading http://www.ti.com/lit/ug/slau720b/slau720b.pdf
3.2 Loading a Configuration
An existing meter configuration can be loaded using the “Load Configuration” button in the main tab as
seen in Figure 7. Some example configurations are available in USS SW Library "example" directory.
Can you please tell me where exactly this directory is located and/or what the configuration file extension might be? I have looked through the C:\ti\msp\USS_02_20_00_16\USS\examples\USSSWLib_template_example folder and it refuses to load any file located in this folder (extensions of .projectspec, .cmd, .ewd, .ewp and .h). Obviously I'm not looking in the correct location but I can find no other folder that was installed with either the USS Design Center or Code Composer Studio that is called "example". Thanks for your help.