Hello,
This is query for just initial level stage for interfacing CC3000 with Tiva TM4C123GH6PM.
And software for patch program is given for TM4C6GH6PGE is it applicable to TM4C123GH6PM ? Or need to do any changes ?
If I want to load Patch program in CC3000, for this I have downloaded all following software please suggest which one do I need to select
This is query for just initial level stage for interfacing CC3000 with Tiva TM4C123GH6PM.
If I want to load Patch program in CC3000, for this I have downloaded all following software please suggest which one do I need to select
- SDK1.11V
- PatchProgrammerLM4F232H5QD_4_11_7_14_24windows_installer
(This is when open in CCs5.5 & on built shows error as follows:
Description Resource Path Location Type
gmake: *** No rule to make target `F:/Ti/PatchProgrammerLM4F232H5QD-4.11.7.14.24/Patch Programmer Source/Patch Programmer CCS/CC3000 Spi/Debug/CC3000 Spi.lib', needed by `Patch Programmer.out'. Patch Programmer Unknown C/C++ Problem )
- Tiva clip-PatchProgrammerLM4F120H5QR-5.11.7.13.19 with this when copy in CCS,
“No error” when import in ccs and change its target to TM4C123GH6pm
- Platform Independent CC3000-Host Driver
( In this swrc263c zip no built in project only header and some c files are there. So do I need to do any changes in this?
Or just need to create new project and merge this all files and compile then load its binary? )
If in this 4th case only binary for CC3000-Host driver there is no CC3000_SPI & Patch programmer Projects included so only one is there CC3000-Host-Driver . So my question is only one is need to load in CC3000 Module of Booster Pack or all others also needed?
I am requesting you to please suggest appropriate way to follow