Hi,
I have Tiva c series TM4C123G LaunchPad Evaluation kit. I'm trying to set priority interrupts that may occur at the same time.Each has a different frequency.(PWM0=10kHz,TIMER=50 kHz).
ADCSequenceConfigure(ADC0_BASE, 0, ADC_TRIGGER_PWM0, 1); //1=lower priority
ADCSequenceConfigure(ADC1_BASE, 1, ADC_TRIGGER_TIMER,0); // 0=higher priority
IntPrioritySet (INT_ADC1SS1, 0); //1=lower priority
IntPrioritySet (INT_ADC1SS1, 1); // 0=higher priority
Is this the same ?
How to enable / disable interrupts in the interrupt ?
What is the difference between these three functions ?
IntPrioritySet()
IntPriorityMaskSet()
IntPriorityGroupingSet()
Thanks for your advice.