Hello,
We recently designed a motor driver board using the DRV8353RH driver chip. Referring to the driver application circuit of the development board, we encountered problems during the test. The problem is that when the motor speed is increased or it is operated at a certain speed for a while, The motor stops rotating and the test FAULT pin is also pulled low. The chip is a hardware configuration interface, we can not know the specific cause of the failure. Is there any way to know the cause of the problem? How to solve this problem. Looking forward to your reply