Hi, is just that i have a Pandaboard ES and i would like to connect the handsfree speaker connector to a speaker (to use the 1.5W amplification from the TWL6040 audio codec), is that possible?, or do i have to decode the output from 13 and 15 pins from the J6 expansion connector from pandaboard, how can i get the an amplified audio output to speaker from that connector (J6)?. thanks.