Hi,
I am facing an issue during suspend & resume, when i am running omap4430 on max performance.
In my project i am using omap4430 & wince
Written a script which place system/device in suspend state after 30 seconds & resumes back after 20 seconds.
Issue is seen randomly on trials. In general it takes 300 to 500 suspend&resume cycles to reproduce the issue. During issue reproduction no external perherials like USB or JTAG were connected.
From the serial logs got to understand that system is hanging as below flow
- PrcmSuspend
- OALCpuLowPower
- OALCPUIdle
after OALCPUIdle is assembly code & not able to debug more. From logs also understood flow is entering into "SaveContext"
Any feedback or pointers will be helpful to resolve the issue.
- gaurav