Hi we are running Android Jelly Bean with kernel version Linux version 3.0.31 on an OMAP4430. We are trying to enable SmartReflex to try and reduce power consumption.
I see in the SmartReflex kernel code that SmartReflex class 3 is only compatible with OMAP343x, is this correct?
We therefore only enabled SmartReflex 1.5 in the kernel. I see that the SmartReflex 1.5 driver gets initialized but I don't know if it is actually working. "omapconf" says that all SmartReflex modules are disabled? Is that expected?
Are there any settings that needs to be tuned to use SmartReflex? How can we verify that SmartReflex is actually working?
Please also note we are using a TWL6032 PMIC. Is there any setup required in the PMIC to enable SmartReflex?
Thanks.