Hello,
I am building "ti-glsdk_dra7xx-evm_6_10_00_02". But it's failing during Yocto Project build. Please help on this.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am building "ti-glsdk_dra7xx-evm_6_10_00_02". But it's failing during Yocto Project build. Please help on this.
Hello Vaibhav,
I remind you that you already have a similar post in our e2e forum.
About you issue with GLSDK:
I saw in the attached file the build environment settings. Your problems are caused by this incorrect settings:
[GLSDK]> PATH is /usr/local/cuda-6.5/bin:/usr/lib/lightdm/lightdm:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/cuda-6.5/bin:/usr/local/cuda-6.5/bin:/home/vaibhav/home/miracast_final/gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux/bin/
[GLSDK]> Building on CPU-194 running Linux CPU-194 3.5.0-54-generic #81~precise1-Ubuntu SMP Tue Jul 15 04:02:22 UTC 2014 x86_64 x86_64 x86_64 GNU/Linux
You must export the cross compiler paths:
export ARCH=arm
export CROSS_COMPILE=/home/users/<username>/gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux/bin/arm-linux-gnueabihf-
export PATH=/home/users/<username>/gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux/bin:$PATH
I think that it is not correct to be used: /usr/local/cuda-6.5/bin:
Please check your proxy settings -
export https_proxy=https://
export http_proxy=http://
export ftp_proxy=http://
sudo GIT_PROXY_COMMAND=/home/users/<username>/bin/git-proxy.sh ./setup.sh
Best regards,
Yanko