Hi All,
I have DRA752 ES 1.1 Jacinto 6 Rev G board, below are the board details. I wanted to use the SD/MMC card slot that is present on the middle board, and found that none of the SD/MMC cards are detected from that port when inserted into that slot. I believe its "mmc3" which indicates status as "disabled" in dra7-evm.dts. Is there any way to enable the Full size SD/MMC (mmc3) card slot on the board ??
U-Boot 2013.04 (Jul 08 2014 - 14:18:21)
CPU : DRA752 ES1.1
Board: DRA7xx
I2C: ready
DRAM: 1.5 GiB
WARNING: Caches not enabled
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
In: serial
Out: serial
Err: serial
Net: cpsw
Hit any key to stop autoboot: 0
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
383 bytes read in 4 ms (92.8 KiB/s)
Running bootscript from mmc0 ...
##
Appreciate your Inputs !
Thanks & Regards,
Skrishna