Hi TI team,
We are using omap5432 MIPI interface to capture camera data, we are able to capture data but encounter a FIFO_OVFIRQ error if MIPI clock rate is too high, the detail is,
OS: linux 3.8
Input bus: FPS:30, 4-lane MIPI CSI2 camera.
format: 8MPixel (3264x2488), raw10.
data path: Sensor ---> ISS ---> Memory.
BURST_SIZE_EXPAND of CSI2_CTRL is 1 and NON_POSTED_WRITE is 1.
When MIPI CLK is less 800M, we can get image well, but when MIPI CLK is higher than 800M, we get csi2 FIFO_OVF_IRQ.
We know omap5432 MIPI supports 1.5Gx4, what can cause the error? ISS or DMA? Is there any way to monitor ISS FIFO/DMA?
Best regards,
Tien-Kuen