Hi,
I am having a similar issue to Dinesh in terms of my IC overheating within my circuit. It seems as though my resistance in my circuit from Vboost to GND is around ~775kΩ before power up. As soon as I power up, the current draw increases to almost 700mA with no load. When checking the same resistance again it has ranged anywhere from 16Ω to 1kΩ depending on the board I've checked on. Either way it is considerably shorter.
The weirdest part is this is the second iteration of the board, and in the first case I had screwed up the resistive divider, but when I modified it and cut traces, I was able to pull my 105V as expected. (Actually running slightly above but still did not see any issues). The only change between the board was correcting the resistor divider and making the board slightly more compact. I'm not sure how this would cause issues though as the board was already compact.
Do you have any idea how this could be occuring?
Thanks,
Kyle