Other Parts Discussed in Thread: TPS2595
Hi TI Team,
We are designing a tracker device which is intended to be placed in Hazardous Zone 0 location. We are following the IEC60079-11 standards to make the device Zone 0 compatible.
The device will be intrinsically safe and we are using Fuse and Zener diode combination to limit the power in case of fault condition.
It is difficult to find the zener diode with Vz~6V and the max input voltage and current 12V and 1.5A respectively. And by placing the current limiter in series with the znener there will be some volatge drop also.
So we cant use the zener diode part in our schematic to limit the voltage in case of fault condition. Does TI has any solution in that case if we want to protect our device in case of overvoltage? Is the IC which we have selected will be suitable for our use?
It would be better if there is a feature in the IC like fail to open instead of fail to short.
Let me know if you need any more details in this regard
Thanks,
Navendu