This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117: LM5117

Part Number: LM5117

Dear All,

We  have designed DC-DC converter using LM5117 IC as per steps given in datasheet. But we are facing some issue while testing it. 

Issue faced:
1) The RT pin is pull down with the resister value of ~22Kohm for getting switching frequency 230Khz. But we got SW freq 110Khz instead of 230Khz.
2) When we applied  36V as Vin, the Output voltage was 14.47V with no load. But on applying 1Amp load, the output voltage dropped to less than 1V.

Below attached is the schematic.

Buck_Coneveter.pdf