Hi,
The data sheet describes the following:
This accuracy is 5%.
Is this accuracy guaranteed within the guaranteed operating temperature(-40℃ to 150℃)?
If not, please provide temperature variation information.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The data sheet describes the following:
This accuracy is 5%.
Is this accuracy guaranteed within the guaranteed operating temperature(-40℃ to 150℃)?
If not, please provide temperature variation information.
Hi Yusuke,
The accuracy is guaranteed over ambient temperature TA = –40°C to the maximum-operating junction temperature TJ = 150°C.
Please notice the the 150°C is junction temperature (TJ).
TPS65381A-Q1 is a grade 1 device which means that the maximum recommended ambient operating temperature 125°C. Operating the device in ambient temperatures above 125°C is not recommended.
Ivan
Hi Ivan,
Thank you for your support.
I understand.
This my question links to the following questions:
https://e2e.ti.com/support/power-management/f/196/t/864258
Customers want graph data showing the relationship between temperature and frequency variation.
Do you have data that shows the relationship between temperature change and frequency change?
Best Regards,
Yusuke
Hello Ivan,
Is there any updates about frequency variation information?
Sorry for rushing you.
Best Regards,
Yusuke
Hi Yusuke-san,
For the system frequency clock parameter we only provide the max and min frequency for TPS65381A-Q1.
Regards,
Ivan