Other Parts Discussed in Thread: BQ25895M, TS3USB221A, BQ25895, BQ24392, BQ24072T
Hello,
I am having some trouble in an implementation which can include my Audio MCU which would communicate when connected to a PC/MAC.
The problem is that the Audio MCU, has two processes (process 1 runs on battery only and process 2 runs on USB only) and it has no proper USB detection, (the only detection it has to switch between the USB and battery is USB 5V detection but it does have enumeration).
The problem occurs that the Audio MCU detects 5V power and immediately switches to process 2 even if its a dedicated charger, but I would like the Audio MCU to continue process 1 during dedicated charging and only go to process 2 when a PC/MAC is detected.
This is why I went with the BQ24160 with its USB detection, but I was wondering can another PHY/USB Audio MCU be connected to the data lines while it is also connected to the BQ24160 for USB detection.
And if so are there extra precautions we need to take on hardware or programming side?
I have attached an simple block image to help understand the idea.
Best regards
Mo