Hello-
I've pasted a waveform to detail this issue. The unseal and full access codes are the default codes. In short, I read the operation status, the pack tells me it is locked. I issue a lock command (a coding error). I issue the unseal command (0414, 3672) and then the full access command (FFFF FFFF). I read the operational status again and the pack is not unlocked. Why did it not unlock???
thanks-
Ray
p.s. So I used the paste from word button and it didn't paste my waveform. So not sure what to do now.
Sure would be nice to be able to attach screen shots or pdfs to these posts.