Hello,
Attached PFC schematic on our board. We are not able to get pwm GDA and GDB. Testing conditions are no load and input AC is 200V. At mentioned testing conditions we measured voltage at
SS (pin no 18) is > 0.6V
VREF (pin 13) = 6V
VSENSE (Pin 4) > 0.75V
VAO (Pin 3) = 0V
Please let us know how to proceed further,according to datasheet VAO should not be 0V, is it correct? Kindly let us know why GDx is not coming and how to proceed.