I am designing a flyback converter with the following specs: Vin: 36-48V(DC), Vout1: 24V(DC) @ 1A. Vout2: 12V(DC) @ 1A. Vout3: 5V @ 1A. Switching Frequency: 50kHZ. I am a student and this is my first time designing one of these. I need a controller for closed loop feedback and to be in a sizeable (DIP) package as we lack facilities to handle the TSSOPS. Thanks.