UCC28910 team,
Working with the UCC28910 EVM, can you give some guidance on how to modify this EVM to support:
Vin: 90VAC to 300VAC
Vout: 12V
Iout: 300mA
I'm hoping this can be done without modifying the transformer.
Thanks,
Darren
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
UCC28910 team,
Working with the UCC28910 EVM, can you give some guidance on how to modify this EVM to support:
Vin: 90VAC to 300VAC
Vout: 12V
Iout: 300mA
I'm hoping this can be done without modifying the transformer.
Thanks,
Darren
Hong,
I might be able to get away with 265VAC max input voltage.
Is there any way the schematic can be modified to use the same transformer and obtain 12v out? Perhaps a voltage divider on the VDD input if the aux winding is providing excessive voltage to VDD? I'm not exactly sure what's preventing it's use, technically.
It is highly desirable to use the same transformer as we will be using it in another device (volume pricing and it's on hand and in stock at our factory), and we know it passes conducted emissions per CE standards.
Thank you,
Eric Wood
Hong,
What are the total transformer changes needed to attain the below ratings. I'd like to continue the conversation with Wurth Electronics.
Vin: 90VAC to 300VAC
Vout: 12V
Iout: 300mA minimum
Thank you,
Eric
The below is obtained based on the UCC28910 design calculation tool for the specified converter using UCC28910.
(1). Converter terminal specifications:
Vin: 90 Vac to 300 Vac
Vout: 12 V
Iout: 300 mA (note: if the Iout > 300 mA, please provide a number so I can re-run the calculation so the below is on the assumption Iout = 300 mA)
(2). Transformer Specifications (Calculation Result):
Primary Inductance: Lp = | 1.61 | mH |
Primary to Secondary Turns Ratio: Nps = | 6.54 | |
Primary to Auxiliary Turns Ratio: Npa = | 4.48 | |
Peak Primary Current: Ip(pk) = | 0.25 | A |
Primary RMS Current: Ip(rms) = | 100 | mA |
Peak Secondary Current: Is(pk) = | 1.65 | A |
Secondary RMS Current: Is(rms) = | 655 | mA |
Maximum Switching Frequency: fsw = | 105 | kHz |
Primary Inductance: Lp = | 1.6 | mH |
Primary to Secondary Turns Ratio: Nps = | 6.54 | |
Primary to Auxiliary Turns Ratio: Npa = | 4.48 | |
Peak Primary Current: Ip(pk) = | 0.25 | A |
Primary RMS Current: Ip(rms) = | 90 | mA |
Peak Secondary Current: Is(pk) = | 1.635 | A |
Secondary RMS Current: Is(rms) = | 403.2 | mA |
Maximum Switching Frequency: fsw = | 100 | kHz |
Hong,
Wurth Electronics suggested the use of p/n: 750312597. Could you please verify if this is suitable for the application? Does the 300VAC max input voltage present any concern? The UCC28910 datasheet suggests 265VAC max, but the web tools suggest 300VAC max.
Thank you,
Eric
The transformer, 750312597, can make the board output 12V and 0.3A with additional changes, based on the UCC28910 calculation sheet:
- Bulk capacitor value increase to > 22uF
- Design full load current = 0.46A, or 5.52W, while only run load up to 0.3A. At 105kHz, the load current is estimated as 0.302A.
If the above sounds good, I will provide all remaining changes based on the UCC28910 calculation sheet.