Hello Team,
I Have meet a problem when I test LED short-circuit on TPS92692EVM, the phenomenon is different from the waveform provided in datasheet.
channel 1 is output of IMON pin, channel 2 is SW wave, and channel3 is the FLT pin output.
When short to GND happened, as shown in below figure, a pulse up to 3.7V on IMON pin appeared and recovered soon, SW wave still exists. and FLT pin was pulled down then pulled high automatically after about 30ms.
A more detailed wave at short circuit is shown as below:
During the short to GND, the device did not hiccup with connecting the FLT pin to the SS pin, and the SW still exists, the FLT pin is high, as shown in below:
I don't know how to solve this problem.
Thanks!