This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. what is the relation between switching frequency and output voltage.
2. how to set the switching frequency in same circuit using Micro controller.
Generally, output voltage is independent of switching frequency. Only the duty cycle is changed for different Vout. It is controlled by the voltage divider in the feedback path. Do you need to switch between two different output voltages of 50 V or 100 V?
sir,
when i am changing the feedback resistor Rfb1 to 730ohm then i am getting 50 V as per simulation. Is it enough to get 50 V with the same circuit in PCB.?
Many of the equations used to determine external components depend on output voltage. So for both 50V and 100 V output, you will need to find compromise values that will work for both. You could possibly simulate both circuits in webench, then adjust the external components so they are the same for both and see if webench suggests any trouble areas.
sir,
what is relation between input voltage and output voltage in DC-DC boost converter. if we change input what will be the output.
sir,
As per WEBENCH the value of Rrc=0.511 Mohm and Crc= 100 pf when switching frequency is 319.105 Khz. but, as per formula same switching frequency and Crc value of Rrc will be 0.0123 ohm.
sir,
What are all possibilities to get negative 50 V output with positive input. which IC i have use for that.