This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTN78060W Output Voltage Power Up 3.5V vs. 3.3V

Other Parts Discussed in Thread: PTN78060W

I have a PTN78060W on three of 500 boards that 20% of the time it will power on with an output voltage of 3.52Vdc vs. 3.31Vdc.  I have attached an excerpt from the schematic.  Input voltage to the circuit = 10.50Vdc.  Input circuit control is a mechanical rocker switch.  I have attached an excerpt from the schematic.  We have been using this PTN for years.  This is an odd anomoly and I am not sure where to start.  Thank you in advance for your time and suggestions.  Circuit load is 0.42 Amps.  - Fred

8206.PTN78060W Schematic.pdf