The query is regarding the battery freshness mode activation.
We are following the below sequence to activated BFM mode
We need to know:
- What is the recommended time till PFI (Step 3) remain high before we execute Step 5 (Drive MR low).
- Also we are facing one issue in which IC is not getting into BFM mode when Battery Voltage (VBAT) is less than 2.9V.
Please guide us regarding the above issues.
The battery freshness seal of the TPS3606 family disconnects the backup battery from the internal circuitry until
it is needed. This ensures that the backup battery connected to VBAT is fresh when the final product is put to
use. The following steps explain how to enable the freshness seal mode:
1. Connect VBAT (VBAT > VBAT(min))
2. Ground PFO
3. Connect PFI to VDD or PFI > V(PFI)
4. Connect VDD to power supply (VDD > VIT)
5. Ground MR
6. Power down VDD
7. The freshness seal mode is entered and pins PFO and MR can be disconnected.
The battery freshness seal mode is disabled by the positive-going edge of RESET when VDD is applied.