Dear everyone.
I was using TPS24751 very useful.
It is great for me to on/off power and to protect overvoltage.
Recently I designed a board that is consume 30A main power.
Because TPS24751 is very useful, I select TPS24751 for new board too.
But TPS24751 is 10A rated, I divided the main power into three parts. (+12.0V_A, +12.0V_B, +12.V_C)
It work well in the first few time. But it seems to be broken at the end.
When last, It is very hot and look like short DRAIN and GND - very large current consume -.
I want to know why this is the result, and wonder how to prevent this result.
I upload my schematic.
Sincery.