Other Parts Discussed in Thread: TMS320C6748, OMAP-L138
I am using a TMDSLCDK6748 evaluation board. I want to configure the SPI communication in the board using SPI0 communication. But only the SPI0_SIMO, SPI0_SOMI and SPI0_SCLK pins are available in the J15 there is no chip select pin out from any of the output jumpers. They seem to be connected to the LAN IC, U23, LAN8710A-EZK. SPI1 communication is available and seems to be connected to the camera header.
Please suggest a way to use the SPI communication in the board.