Part Number: TMDXEVM8148
Good day to u,
I want to create an application in CCS v5.5 for the TMDXEVM8148 that will be able to detect some faces and match them with a database.
So I have in mind using Syslink to be able to communicate between the ARM processor and the DSP. My plan is that ARM will "send" the image to the DSP that will do some black magic woodoo and return the result.
So my question is do I have to build Syslink and install it ?
Because what i don't understand is that on my target when i do lsmod, the module Syslink is already here: :(
Module Size Used by
bufferclass_ti 4950 0
omaplfb 10794 0
pvrsrvkm 155618 2 bufferclass_ti,omaplfb
tlc59108 1545 0
ti81xxhdmi 17685 0
ti81xxfb 21979 1
vpss 74936 3 omaplfb,ti81xxhdmi,ti81xxfb
syslink 1133911 0
ipv6 214095 16
Btw I'm on ubuntu 10.04, with EZSDK 5.05.02.00
Hoping that I'm clear enough,
Thx in advance,
Marc