Part Number: DRA74
What is the recommended power solution for DRA74x, DRA75x, or TDA2x?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There are three recommended power configurations for the DRA74x, DRA75x, and TDA2x devices.
The details of these configurations are listed in the TPS659039-Q1 user’s guide for DRA74x, DRA75x, and TDA2x.
For low-power use cases of the DRA74x, DRA75x, and TDA2x processors, the TPS65917-Q1 can be used instead, along with TPS22965-Q1 and TPS51200-Q1. The TPS65917-Q1 supports processor currents up to 3A on the MPU rail, and 3A on the DSPEVE + GPU + IVA rails combined. The details of these configurations are listed in the TPS65917-Q1 User’s Guide to Power DRA7xx and TDA2x/TDA2Ex.