MCU is AM3352 300MHZ
the old NAND FLASH is MT29F1G08ABAEAWP, and the new one is MT29F2G08ABAGAWP-IT:G,
the system can work well using the old flash, but use the new one, have some probability to boot fail (about 30% ~ 40%). and if boot sucess, the system also can work well.
what's the problem? timing between NANDFLASH and BOOTROM code?
SYSBOOT config is: 0100000000001011