Hi,
I'am using TI AM5728 IDK, P/N: 296-46780-ND kit with Linux SDK ver:05.03.00.07(i.e ti-processor-sdk-linux-am57xx-evm-05.03.00.07-Linux-x86-Install.bin).
I want to build the SDK for NOR image.
1. How to enable the NOR build
2. where to specify the NOR Flash Image Layout. It should have sections like: Uboot, Kernel, RootFs, Application.
3. How to define the flash section for Application in the NOR.
4.Which linker scatter file I've to update for sections.
5. please specify the location of static libraries, .so files, .KO(kernel objects), exe files. simple example Makefile.
Thanks and Regards
srinivasa