Hi.
I am not using CCS to realize the labs because I don't have a JTAG :(
I successfully realized previous PRU labs, but I can't get Lab 3 to work.
Both firmwares compile and are loaded by PRUs, but the expected behaviour (red LED for warming and blue LED for cooling) doesn't occur.
Which pins must be in which mode to get Lab 3 working? I'm using the following:
P8_30 pruout OUT_1WIRE on code temp_monitor_slave_0.c for PRU0 (PR1_PRU_EDIO_DATA_OUT5) P8_16 pruin IN_1WIRE on code temp_monitor_slave_0.c for PRU0 (PR1_PRU0_GPI14) P8_44 pruout GPIO_BLUE on code temp_monitor_slave_1.c for PRU1 (PR1_PRU1_GPO3) P8_42 pruout GPIO_RED on code temp_monitor_slave_1.c for PRU1 (PR1_PRU1_GPO5) P8_41 pruout GPIO_GREEN on code temp_monitor_slave_1.c for PRU1 (PR1_PRU1_GPO4)
Thanks in advance.