Hello Champs,
The GP EVM and StarterKit schematic are different when using USB0 in DRD mode.
In Starterkit board, the USB0_ID is connected to NMOS Q9 which connected to GPMC_WAIT0. While in GP EVM schematic, the USB0_ID is not brought out, the VUSB_VBUS0 is connected to NMOS Q2 instead, the NMOS Q2 is connected to GPIO_13.
Which one is correct? What the function of NMOS?
Below are the GP EVM and StarterKit schematic.
StarterKit schematic
GP EVM schematic