This is a very similar question to https://e2e.ti.com/support/processors/f/791/t/864118?tisearch=e2e-sitesearch&keymatch=beaglebone%25252525252525252520ai (It seems that the "Ask a related question" functionality is broken on the forum). Slightly different from this question, however, since this version of the TI PDSK supports the BeagleBone AI.
Basically, I have a BeagleBone AI and I have just flashed an SD card with the latest TI PSDK image for Linux. Upon inserting into the microSD card slot on the BBAI, holding down RESET button, plugging into power, and releasing RESET, the board doesn't boot. The power LED comes on, but none of the other 5 status LEDs do (https://github.com/beagleboard/beaglebone-ai/wiki/System-Reference-Manual#user-leds), as they normally would with the Debian image provided by BeagleBoard.
Any help is much appreciated -- thanks!
Matt