Hello,to whom it may concern,
The fvco is 4300MHz~5376MHz in the datasheet(p6).
But Approximate VCO Ranges is 4200MHz~5520MHz in the datasheet(p42).
Which is correct of p6 and p42?
Best regards,
Manabu Ito
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Manabu,
The Frequency range for the VCO is 4300MHz-5376MHz.
Best Regards,
Julian
If my post answers your question, please click on "Verify Answer" button.
Hi Manabu
Table 40 shows approximate VCO values. They may vary slightly in different devices.
While the table shows 4200-5520 MHz, the actual VCO frequency range has to be wider in order to guarantee VCO frequency range is between 4300M – 5376MHz.
We can only guarantee that the device will work on the 4300MHz-5376MHz range as shown in the Electrical Characteristics table.
Thanks,
Julian
If my post answers your question, please click on "Verify Answer" button.