I have a TMP007 EVM and the corresponding GUI. I am setting the power on, then setting device configuration up to be:
Conversion mode = Convert Local & Obj.
Total Conversion Time = 4 Sec (Idle for 3.5).
Transient Correction = Enable.
Then clearing both graphs on the "Temperature Limit Controls" tab, setting them to autoscale both X & Y and then starting Continuous Read.
The problem I have is both graphs start updating at a rate far quicker than once every 4 seconds and exporting to excel creates a lot more data than I want. It is as if the setting for Total Conversion Time is not being sent from the GUI to the sensor.
I've read the guide for the GUI and I can't see where I'm going wrong. Can anyone help? Thanks.