Dear all,
We would like you to check circuit diagram.
Please see attachment file.
This pin has absolute maximum about voltage and current value.
Is this circuit OK?
LM73 absolute maximum ratings.pdf
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all,
We would like you to check circuit diagram.
Please see attachment file.
This pin has absolute maximum about voltage and current value.
Is this circuit OK?
LM73 absolute maximum ratings.pdf
Best regards,
Hi Yamamoto-san,
The diode which you drew, titled "Equivalent Circuit," is wrong. This does not exist in LM73. Page 3 of the LM73 datasheet has illustrations for the CLK and DAT pins. Additionally, Page 4 explicitly states, in 6.1 Absolute Maximum Ratings, that CLK and DAT pins may go up to 6V regardless of Vdd. This is the correct way to build an SMBus/I2C compliant device. Not all devices are created this way. The bus is defined this way such that pull-up resistors create the logic high while devices can only pull down to create logic low. This has the added benefit that mixed logic levels can co-exist without the need for level shifters as you have suggested. I'm attaching an illustration below which shows how this system should be implemented.
Thanks,
Ren