Hello,
I am running the capture demo on IWR1443BOOST with SDK MMWAVE_SDK_01_01_00_02. I can trigger the capture through terminal, connect the board via CCS, save gDataCube to a file, and see the ADC and range data via capture_demo.m file in MATLAB. However, when I need to trigger the capture again (after disconnecting from CCS), I need to reset the board via pressing the NRST switch; otherwise, the next trigger gives 'Error -1".
Is there any way to use a software command as a substitute for the NRST hardware switch pressing?
Thanks,
Sanjib